Solid Edge FrameworkSupport Type Library
SendToBack Method
Description
Changes the display order of visible objects by moving the referenced object behind all overlapping objects.
Syntax
Visual Basic
Public Sub SendToBack() 
Remarks
This command is useful when objects are hiding other objects that have a lower priority display. The SendBackward method can also be used.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame
    ' Local variables to be declared here
    Dim lngZorder As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Draw few entities prior to the FeatureControlFrame
    Call objSheet.Lines2d.AddBy2Points(x1:=0.125, y1:=0.1, x2:=0.275, y2:=0.25)
    Call objSheet.Lines2d.AddBy2Points(x1:=0.2, y1:=0.25, x2:=0.3, y2:=0.125)
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Add a new FeatureControlFrame
    Set objFCF = objFCFs.Add(x:=0.1, y:=0.1, z:=0)
    objFCF.PrimaryFrame = "FLVB0.001MCVBA"
    Call objFCF.AddVertex(x:=0.2, y:=0.2, z:=0)
    objFCF.BreakLine = True
    'Get the Zorder of the FeatureControlFrame
    lngZorder = objFCF.ZOrder
    'Place the FCF back of all entities that are obscuring it
    Call objFCF.SendToBack
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objFCFs = Nothing
    Set objFCF = Nothing
End Sub
See Also

FeatureControlFrame Object  | FeatureControlFrame Members