Solid Edge FrameworkSupport Type Library
Style Property
Description
For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only.
Property type
Read-only property
Syntax
Visual Basic
Public Property Style As DimStyle
Example
Private Sub Form_Load()

    Dim objApp As SolidEdgeFrameWork.Application

    Dim objDoc As SolidEdgeDraft.DraftDocument

    Dim objSheet As SolidEdgeDraft.Sheet

    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames

    Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame

    Dim objFCFStyle As SolidEdgeFrameworkSupport.DimStyle

    ' Local variables to be declared here
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")

        objApp.Visible = True

    Else

        Set objDoc = objApp.ActiveDocument

    End If

    On Error GoTo 0

    'Get the Active Sheet object

    Set objSheet = objDoc.ActiveSheet

    'Get the FeatureControlFrames collection object

    Set objFCFs = objSheet.FeatureControlFrames

    'Add a new FeatureControlFrame

    Set objFCF = objFCFs.Add(x:=0.1, y:=0.1, z:=0)

    objFCF.PrimaryFrame = "FLVB0.001MCVBA"

    Call objFCF.AddVertex(x:=0.2, y:=0.2, z:=0)

    objFCF.BreakLine = True

    'Get the DimStyle associated with the FCF

    Set objFCFStyle = objFCF.Style

    ' Release objects

    Set objApp = Nothing

    Set objDoc = Nothing

    Set objSheet = Nothing

    Set objFCFs = Nothing

    Set objFCF = Nothing

    Set objFCFStyle = Nothing

End Sub
See Also

FeatureControlFrame Object  | FeatureControlFrame Members