Solid Edge FrameworkSupport Type Library
FlipVertical Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
Image2d Object
: FlipVertical Property
Description
This read-write Boolean property flips the vertical orientation of the referenced Image2d object.
Property type
Read-write property
Syntax
Visual Basic
Public Property FlipVertical As Boolean
Remarks
When this property is True, the vertical orientation is flipped; when False, it is not.
See Also
Image2d Object
|
Image2d Members