Angle | The angular rotation of the referenced object. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BorderColor | Gets and sets the border color as a COLORREF int. |
BorderStyleName | Gets and sets the linear style name of the border. |
BorderTypeName | Gets and sets the dash style name of the border. |
BorderWidth | Gets and sets the width of the border in mm. |
FlipHorizontal | This read-write Boolean property flips the horizontal orientation of the referenced Image2d object. |
FlipVertical | This read-write Boolean property flips the vertical orientation of the referenced Image2d object. |
Height | Returns the height of the referenced object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsLink | Specifies whether or not the file associated with the referenced object was inserted as an OLE link. |
Layer | Sets and returns the named layer on which the referenced object resides. |
LockAspectRatio | This read-write Boolean property specifies whether the aspect ratio of the referenced Image2d object is locked. When set to True, the Height and Width of the referenced Image2d object retain the same proportions when either of them is changed. |
Opacity | Sets and returns the opacity (from 0% to 100%) for the referenced Image2d object. |
Parent | Returns the parent object for the referenced object. |
ResetAspectRatio | This read-write Boolean property specifies whether the aspect ratio of the referenced Image2d object is reset. When set to True, the Height and Width of the referenced Image2d object return to their original proportions. |
ShowBorder | Gets and sets TRUE/FALSE for ShowBorder enabled/disabled |
Type | Specifies the type of the object being referenced. |
Width | Returns the width of the referenced object. |