Solid Edge FrameworkSupport Type Library
LockAspectRatio Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
Image2d Object
: LockAspectRatio Property
Description
This read-write Boolean property specifies whether the aspect ratio of the referenced Image2d object is locked. When set to True, the Height and Width of the referenced Image2d object retain the same proportions when either of them is changed.
Property type
Read-write property
Syntax
Visual Basic
Public Property LockAspectRatio As Boolean
See Also
Image2d Object
|
Image2d Members