Solid Edge FrameworkSupport Type Library
Opacity Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
Image2d Object
: Opacity Property
Description
Sets and returns the opacity (from 0% to 100%) for the referenced Image2d object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Opacity As Integer
See Also
Image2d Object
|
Image2d Members