Solid Edge FrameworkSupport Type Library
BeforeSpacing Property
Description
Sets and returns the amount of space above the first line of the paragraph for the referenced text object.
Property type
Read-write property
Syntax
Visual Basic
Public Property BeforeSpacing As Double
Remarks
The TextEdit object always has an insert index or a selection active; setting any property on the TextEdit object applies to the current selection (if present) or to the text at the current insert index.
See Also

TextEdit Object  | TextEdit Members