AfterSpacing | Sets and returns the amount of space below the first line of the paragraph for the referenced text object. |
AspectRatio | Sets and returns the character width-to-charager height ratio. |
BeforeSpacing | Sets and returns the amount of space above the first line of the paragraph for the referenced text object. |
Bold | Specifies whether or not the associated text is bold. |
Bullet | Specifies whether or not paragraph bulleting is turned on. |
Characters | Sets and returns character data for the referenced TextEdit object. |
CharacterSpacing | Sets and returns the spacing between characters for the associated text. |
Color | Sets or returns the color of the referenced text. |
FirstLineIndent | Sets and returns the distance from the margin to the start of the line. |
Font | Sets and returns the name of the font. |
HorizontalAlignment | Sets and returns the horizontal alignment of the text within a paragraph. |
InsertIndex | Sets and returns the index at which the next character will be inserted for the referenced TextEdit object. |
IsEmpty | Specifies whether or not the referenced object is empty. |
Italic | Specifies whether or not the associated text is italic. |
Language | Sets and returns the language in which the text is written. |
LeftIndent | Sets and returns the distance from the left margin to the end of the line. |
LineSpacing | Sets and returns the amount of space between two lines in a paragraph for the referenced object. |
LineSpacingType | Sets and returns the Line Spacing type for the referenced TextBox object. |
Name | Returns the name of the referenced object. |
Number | Specifies whether or not paragraph numbering is turned on. |
NumberingStartValue | Sets the start value for the referenced numbered list |
RightIndent | Sets and returns the distance from the right margin to the end of the line. |
SpecialIndentType | Sets and returns the Special Indent type None, First line, or Hanging |
SubScript | Specifies whether or not the associated text is subscripted. |
SuperScript | Specifies whether or not the associated text is superscripted. |
TextScale | Sets and returns the text scale of the object. |
TextSize | Sets and returns the size of the text for the referenced object. |
UnderLine | Specifies whether or not the associated text is underlined. |
VerticalPosition | Sets and returns the vertical position of superscript and subscript text. |