Solid Edge FrameworkSupport Type Library > TextEdit Object : InsertFraction Method |
Visual Basic |
---|
Public Sub InsertFraction( _ ByVal UpperText As String, _ ByVal LowerText As String, _ ByVal typeOption As TextFractionTypeConstants, _ ByVal alignOption As TextFractionAlignConstants, _ ByVal fractionSize As TextFractionSizeConstants _ ) |
Value | Description |
---|---|
igLinearFraction | Text Fraction Linear Type |
igSkewed | Text Fraction Skewed Type |
igStacked | Text Fraction Stacked Type |
igTolerance | Text Fraction Tolerance Type |
Value | Description |
---|---|
igLower | Text Fraction Align Lower Type |
igMiddle | Text Fraction Align Middle Type |
igUpper | Text Fraction Align Upper Type |
Value | Description |
---|---|
ig10 | Text Fraction Size 10 |
ig100 | Text Fraction Size 100 |
ig20 | Text Fraction Size 20 |
ig30 | Text Fraction Size 30 |
ig40 | Text Fraction Size 40 |
ig50 | Text Fraction Size 50 |
ig60 | Text Fraction Size 60 |
ig70 | Text Fraction Size 70 |
ig80 | Text Fraction Size 80 |
ig90 | Text Fraction Size 90 |