Solid Edge FrameworkSupport Type Library
VerticalPosition Property
Description
Sets and returns the vertical position of superscript and subscript text.
Property type
Read-write property
Syntax
Visual Basic
Public Property VerticalPosition As Double
Remarks
The TextEdit object always has an insert index or an active selection. Setting any property on the TextEdit object applies to the current selection, if one is present, or to the text at the current insert index.
See Also

TextEdit Object  | TextEdit Members