Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BottomNote1 | Sets and returns the Bottom Note 1 text for the referenced object. |
BottomNote2 | Sets and returns the Bottom Note 2 text for the referenced object. |
BottomNote3 | Sets and returns the Bottom Note 3 text for the referenced object. |
BottomNoteAngle | |
BottomNoteCSize | |
BottomNoteDepth | |
BottomNoteZ | Sets and returns the Bottom Note Z text for the referenced object. |
BottomPosOffset | |
BottomTreatmentType | Sets and returns the treatment display style to use for the bottom treatment portion of the referenced object. |
BottomType | Sets and returns the bottom type for the referenced object. |
BottomWeldModifier | Sets and returns the bottom weld modifier for the referenced object. |
BreakLine | Specifies whether or not a breakline is added between the leader line and the referenced dimensioning object. |
BreakLineDirection | Sets and returns the direction (left or right) in which the break line runs along the x axis. |
BreakLineDistance | Sets and returns the length along the x axis that the break line traverses. |
DashLine | Sets and returns the relative position of the dash lines for the referenced weld symbol object. |
Document | Returns the document to which the referenced object belongs. |
HidePMI | Show or Hide the referenced PMI Weld Symbol object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Leader | Specifies whether or not the referenced object has a leader line. |
Name | Returns the name of the referenced object. |
OffsetTopBottom | Specifies whether the top and bottom weld types are offset or aligned. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
PMIName | Get and set the name of reference PMI annotation object. |
PMIPlane | |
PMITrackDistance | |
RotationAngle | Sets and returns the angle, in radians, at which the object is rotated along its major axis. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
Symmetrical | Specifies whether or not the referenced object is symmetrical. |
Tail | Specifies whether the less than symbol appears at the end of the breaklline. |
TailNote | Sets and returns the tail note text. |
TailNote2 | Sets and returns the tail note text for the referenced object. |
TextScale | Sets and returns the text scale of the object. |
TopNote1 | Sets and returns the Top Note 1 text. |
TopNote2 | Sets and returns the Top Note 2 text. |
TopNote3 | Sets and returns the Top Note 3 text. |
TopNoteAngle | |
TopNoteCSize | |
TopNoteDepth | |
TopNoteZ | Sets and returns the Top Note Z text. |
TopPosOffset | |
TopTreatmentType | Sets and returns the display style to use for the top treatment portion of the referenced object. |
TopType | Sets and returns the top type for the referenced object. |
TopWeldModifier | Sets and returns the top weld modifier for the referenced object. |
Type | Specifies the type of the object being referenced. |
VertexCount | Returns the number of vertices in the referenced object. |
WeldAllAround | Specifies whether or not the 'weld all around' display style is included in the referenced object. |
WeldInField | Specifies whether or not the 'weld in field' display style is included in the referenced object. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |
ZSymbol | Specifies whether or not the Z weld symbol modifier is included in the referenced object. |