Solid Edge FrameworkSupport Type Library
RemoveVertex Method
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
WeldSymbol Object
: RemoveVertex Method
Specifies the index, relative to zero of the vertex number in the Linestring. This value must be between one and the number of vertices.
Description
Removes a vertex at a specified index, causing indices of following vertices to decrement by one.
Syntax
Visual Basic
Public Sub RemoveVertex( _ ByVal
Index
As Long _ )
Parameters
Index
Specifies the index, relative to zero of the vertex number in the Linestring. This value must be between one and the number of vertices.
See Also
WeldSymbol Object
|
WeldSymbol Members