Solid Edge Framework Type Library
OnCommandUpdateUI Event
The command identifier for the affected command.
Enables or disables the command. Values are as follows: seCmdActive_Enabled (enables the command), seCmdActive_Checked (adds a check mark on the command's active window), seCmdActive_ChangeText (changes the text that appears on the command's menu item), seCmdActive_UseDotMark (adds a dot mark on the command's menu item), or seCmdActive_UseBitmap (displays the command's menu item as a bitmap).
Description
Occurs when the user interface needs to be updated.
Syntax
Visual Basic
Public Event OnCommandUpdateUI( _
   ByVal nCmdID As Long, _
   ByRef lCmdFlags As Long, _
   ByRef MenuItemText As String, _
   ByRef nIDBitmap As Long _
)
Parameters
nCmdID
The command identifier for the affected command.
lCmdFlags
Enables or disables the command. Values are as follows: seCmdActive_Enabled (enables the command), seCmdActive_Checked (adds a check mark on the command's active window), seCmdActive_ChangeText (changes the text that appears on the command's menu item), seCmdActive_UseDotMark (adds a dot mark on the command's menu item), or seCmdActive_UseBitmap (displays the command's menu item as a bitmap).
MenuItemText
The text that appears on the menu.
nIDBitmap
See Also

AddInEvents Object  | AddInEvents Members