Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objBaseProfile(1 To 2) As SolidEdgePart.Profile
Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
Dim objArc1 As SolidEdgeFrameworkSupport.Arc2d
Dim objArc2 As SolidEdgeFrameworkSupport.Arc2d
Dim objModel As SolidEdgePart.Model
Dim objExtProtrusion As SolidEdgePart.ExtrudedProtrusion
Dim objRelations As SolidEdgeFrameworkSupport.Relations2d
Dim objAttributeSet As Object
Dim objAttribute As Object
Dim lngStatus As Long
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
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
'Create an Extruded Protrusion as Base feature
Set objBaseProfile(1) = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
Set objLine1 = objBaseProfile(1).Lines2d.AddBy2Points(x1:=0.05, y1:=0, x2:=0.05, y2:=0.15)
Set objArc1 = objBaseProfile(1).Arcs2d.AddByCenterStartEnd(xCenter:=0.025, yCenter:=0.15, _
xStart:=0.05, yStart:=0.15, xEnd:=0, yEnd:=0.15)
Set objLine2 = objBaseProfile(1).Lines2d.AddBy2Points(x1:=0, y1:=0.15, x2:=0, y2:=0)
Set objArc2 = objBaseProfile(1).Arcs2d.AddByCenterStartEnd(xCenter:=0.025, yCenter:=0, _
xStart:=0, yStart:=0, xEnd:=0.05, yEnd:=0)
Set objRelations = objBaseProfile(1).Relations2d
objRelations.AddKeypoint Object1:=objLine1, Index1:=igLineEnd, Object2:=objArc1, Index2:=igArcStart
objRelations.AddKeypoint Object1:=objArc1, Index1:=igArcEnd, Object2:=objLine2, Index2:=igLineStart
objRelations.AddKeypoint Object1:=objLine2, Index1:=igLineEnd, Object2:=objArc2, Index2:=igArcStart
objRelations.AddKeypoint Object1:=objArc2, Index1:=igArcEnd, Object2:=objLine1, Index2:=igLineStart
lngStatus = objBaseProfile(1).End(ValidationCriteria:=igProfileClosed)
If lngStatus <> 0 Then
MsgBox ("Base feature profile is not closed")
End If
Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, ProfileArray:=objBaseProfile, _
ProfilePlaneSide:=igRight, ExtrusionDistance:=0.05)
objBaseProfile(1).Visible = False
Set objExtProtrusion = objModel.ExtrudedProtrusions(1)
If objExtProtrusion.Status <> igFeatureOK Then
MsgBox "Base Feature is not created properly"
End If
'Create an AttributeSet with Add method
Set objAttributeSet = objExtProtrusion.AttributeSets.Add("MyAttrib Set")
'CASE 1 - a single attribute
'Add an Attribute to the set with Add method
Set objAttribute = objAttributeSet.Add("Attribute1", vbInteger)
If objAttribute.Name <> "Attribute1" Or objAttribute.Type <> vbInteger Then
MsgBox "Add method of AttributSet failed"
End If
'CASE 2 - Create an array of Attribute
'Add an Attribute to the set with Add method
Set objAttribute = objAttributeSet.Add("Attribute2", vbCurrency, 5)
If objAttribute.Name <> "Attribute2" Or objAttribute.Type <> vbArray + vbCurrency Or objAttribute.Dimension <> 5 Then
MsgBox "Add method of AttributSet with Subscript failed"
End If
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objBaseProfile(1) = Nothing
Set objBaseProfile(2) = Nothing
Set objLine1 = Nothing
Set objLine2 = Nothing
Set objArc1 = Nothing
Set objArc2 = Nothing
Set objModel = Nothing
Set objExtProtrusion = Nothing
Set objRelations = Nothing
Set objAttributeSet = Nothing
Set objAttribute = Nothing
End Sub