Solid Edge Framework Type Library
OnAction Property
Description
Sets or returns the name of the macro to run when the user clicks a command bar control or when the Execute method on the control is run.
Property type
Read-write property
Syntax
Visual Basic
Public Property OnAction As String
See Also

CommandBarPopup Object  | CommandBarPopup Members