Solid Edge Framework Type Library
ActiveMenuBar Property
Description
Returns the active menu bar.
Property type
Read-only property
Syntax
Visual Basic
Public Property ActiveMenuBar As CommandBar
Remarks
The active menu bar is the command bar serving as the primary menu. This is the menu that contains the standard menu items such as File, Edit, View, and so forth.
See Also

CommandBars Collection  | CommandBars Members