Solid Edge Framework Type Library
LargeButtons Property
Description
Specifies whether or not large buttons are displayed for the referenced CommandBar object.
Property type
Read-write property
Syntax
Visual Basic
Public Property LargeButtons As Boolean
Remarks
If True, large buttons are displayed. If False, normal-size buttons are displayed. This property affects all command bars within the application, not just the command bars within the parent environment.
See Also

CommandBars Collection  | CommandBars Members