Solid Edge Framework Type Library
Customization Object Members
Overview 
Public Methods
Public Method BeginCustomizationMust call this method at the start of customization.
Public Method EndCustomizationMust call this method at the end of customization to free up resources.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property ParentReturns the parent object for the referenced object.
Public Property RadialMenuReturns the RadialMenus collection object, which is used to customize the radial menu layout.
Public Property RibbonBarThemesReturns the RibbonBarThemes collection object, which is used to customize the ribbon bar layout.
Public Property SwitchWindowCustReturns the SwitchWindow collection object.
See Also

Customization Object  | Solid Edge ST3 - What's New