Solid Edge Framework Type Library
BeforeCommandRun Method
The ID of the command for which the event is triggered.
Description
Occurs before a specified command is run.
Syntax
Visual Basic
Public Sub BeforeCommandRun( _
   ByVal theCommandID As Long _
) 
Parameters
theCommandID
The ID of the command for which the event is triggered.
See Also

DISEApplicationEvents Object  | DISEApplicationEvents Members