Solid Edge Framework Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEnvironments As SolidEdgeFramework.Environments
    Dim objEnvironment As SolidEdgeFramework.Environment
    Dim objEnvApplication As SolidEdgeFramework.Application
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Environments collection
    Set objEnvironments = objApp.Environments
    'Get the Part environment i.e., 9th item in the Environments collection
    Set objEnvironment = objEnvironments(9)
    'Get the Application from Environment
    Set objEnvApplication = objEnvironment.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEnvironments = Nothing
    Set objEnvironment = Nothing
    Set objEnvApplication = Nothing
End Sub
See Also

Environment Object  | Environment Members