Solid Edge Framework Type Library
Name Property
Description
Returns the name of the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Name As String
Remarks
All objects have names that are unique within the scope of their parent.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objEnvironments As SolidEdgeFramework.Environments
    Dim objEnvironment As SolidEdgeFramework.Environment
    Dim strName As String
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the Environments collection
    Set objEnvironments = objApp.Environments
    'Get the Part environment i.e., 9th item in the Environments collection
    Set objEnvironment = objEnvironments(9)
    'Get the Name of the Environment
    strName = objEnvironment.Name
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objEnvironments = Nothing
    Set objEnvironment = Nothing
End Sub
See Also

Environment Object  | Environment Members