Solid Edge Framework Type Library
BumpmapInvert Property
Description
Sets and returns a flag used on the bump map in the referenced FaceStyle object. If the flag is true, the bump map's bumps will invert, so that the high points will look like holes instead of bumps.
Property type
Read-write property
Syntax
Visual Basic
Public Property BumpmapInvert As Long
See Also

FaceStyle Object  | FaceStyle Members