Solid Edge Framework Type Library
SkyboxClear Method
The side from which the image is cleared.
Description
Clears the image from one side of the skybox in the referenced FaceStyle object.
Syntax
Visual Basic
Public Sub SkyboxClear( _
   ByVal nSide As Integer _
) 
Parameters
nSide
The side from which the image is cleared.
See Also

FaceStyle Object  | FaceStyle Members