Solid Edge Framework Type Library
SkyboxConeAngle Property
Description
Sets and returns the cone angle of the skybox used in the referenced FaceStyle object.
Property type
Read-write property
Syntax
Visual Basic
Public Property SkyboxConeAngle As Single
Remarks
The cone angle is like a camera's field of view angle. Small values zoom to a tight focus on a small area of the skybox, and large values show a wide area of the skybox. Values must be greater than 0 degrees and less than 180 degrees.
See Also

FaceStyle Object  | FaceStyle Members