Solid Edge Framework Type Library
TextureTransparent Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
FaceStyle Object
: TextureTransparent Property
Description
Sets and returns a flag used on the texture map in the referenced FaceStyle object. If the flag is true, the texture will be transparent wherever its pixels are the transparent color, otherwise the texture will be completely opaque.
Property type
Read-write property
Syntax
Visual Basic
Public Property TextureTransparent As Long
See Also
FaceStyle Object
|
FaceStyle Members