Solid Edge Framework Type Library
TextureUnits Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
FaceStyle Object
: TextureUnits Property
Description
Sets and returns the units used for texture scaling. When it is set to 1, the scaling factors will be in world coordinates, which are the default. When it is set to 2, the scaling is in surface coordinates.
Property type
Read-write property
Syntax
Visual Basic
Public Property TextureUnits As Integer
See Also
FaceStyle Object
|
FaceStyle Members