AddHatch | Creates a linear element to be used in the referenced hatch pattern. |
AddHatchWithOption | Same as AddHatch with extra option for creating linear or radial element and center location and axis ratio if radial element |
GetColor | Returns the color currently applied to a specified linear element used in a HatchPatternStyle object. |
GetDashGap | Returns the dash and gap characteristics of the referenced style object. |
GetDashType | Returns the linear style that is currently applied to a specified linear element used in a HatchPatternStyle object. |
GetElementType | Get the element type - Linear or Radial |
GetHatch | Returns the parameters for the referenced hatch line. |
GetHatchWithOption | Same as GetHatch with extra option for getting linear or radial element and center location and axis ratio if radial element |
GetOrigin | Returns the origin for the referenced object. |
GetRadialElementAxisRatio | Get the axis ratio of ellipse for radial elements |
GetRadialElementCenterLocation | Get the location of ellipse center for radial elements |
GetRotation | Returns the rotation of the reference hatch line. |
GetShift | Returns the shift of the specified hatch line. |
GetSpacing | Returns the spacing of the specified hatch line. |
GetWidth | Returns the width of the specified hatch line. |
RemoveHatch | Removes the specified hatch line from the referenced HatchPatternStyle object. |
SetColor | Specifies a new color for a specified linear element used in a HatchPatternStyle object. |
SetDashGap | Defines the dash and gap characteristics of a linear element. |
SetDashType | Specifies the new linear style to apply to a specified linear element used in a HatchPatternStyle object. |
SetDisplayIndex | Changes the display index number of an element. |
SetElementType | Set the element type - Linear or Radial |
SetHatch | Modifies one or more characteristics of an existing linear element used in a hatch pattern. |
SetHatchWithOption | Same as SetHatch with extra option for setting linear or radial element and center location and axis ratio if radial element |
SetMasterColor | Changes the color of each hatch line in the referenced HatchPatternStyle object. |
SetMasterWidth | Changes the width of each hatch line in the referenced HatchPatternStyle object. |
SetOrigin | Redefines the offset between the lower left corner of the window and the object's origin. |
SetRadialElementAxisRatio | Set the axis ratio of ellipse for radial elements |
SetRadialElementCenterLocation | Set the location of ellipse center for radial elements |
SetRotation | Specifies a new angle of rotation for a specified linear element used in a HatchPatternStyle object. |
SetShift | Sets the shift of the specified hatch line. |
SetSpacing | Specifies a new horizontal distance at which a specified linear element used in a HatchPatternStyle object is repeated. |
SetWidth | Sets the width of the specified hatch line. |