Solid Edge Framework Type Library
WindowProc Method
Specifies the window handle.
Specifies the message.
Specifies additional message information.
Specifies additional message information.
Description
Occurs when the application receives a window event.
Syntax
Visual Basic
Public Function WindowProc( _
   ByVal hWnd As Long, _
   ByVal nMsg As Long, _
   ByVal wParam As Long, _
   ByVal lParam As Long _
) As HResult
Parameters
hWnd
Specifies the window handle.
nMsg
Specifies the message.
wParam
Specifies additional message information.
lParam
Specifies additional message information.
See Also

ISEApplicationWindowEvents Object  | ISEApplicationWindowEvents Members