Solid Edge Framework Type Library
DisplayTooltips Property
Collapse All
Expand All
Solid Edge Framework Type Library
>
ISECommandBars Collection
: DisplayTooltips Property
Description
Specifies whether or not Tool Tips are displaye for the referenced CommandBar object.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayTooltips As Boolean
Remarks
This property affects all command bars within the application, not just the command bars within the parent environment.
See Also
ISECommandBars Collection
|
ISECommandBars Members