Solid Edge Framework Type Library
BeforeModelIsDeleted Method
The Model object for which the event is triggered.
Description
Occurs before a specified model is deleted.
Syntax
Visual Basic
Public Function BeforeModelIsDeleted( _
   ByVal Model As Object _
) As HResult
Parameters
Model
The Model object for which the event is triggered.
See Also

ISEModelRecomputeEvents Object  | ISEModelRecomputeEvents Members