Solid Edge Framework Type Library
MouseClick Method
Specifies on which button the click occurred. Valid values are vbLeftButton, vbRightButton, or vbMiddleButton.
Bitmask that determines the states of the Ctrl, Shift, and Alt keys when the mouse was clicked. For example, if both the Ctrl and Shift keys are pressed, the value is 6.
Returns the x coordinate of the mouse in either the window or model coordinate system, depending on the value of the ScaleMode property.
Returns the y coordinate of the mouse in either the window or model coordinate system, depending on the value of the ScaleMode property.
Returns the z coordinate of the mouse in the model coordinate system if the scale mode property is set to igMouseModel and the mouse event occurred in a graphic view; otherwise 0.
Returns the window object in which the click event occurred.
If the mouse is over a graphic object when the mouse event occurs and the underlying application supports automatic key-point snapping, then this argument contains the index of the key point. Key points are significant points such as the center of a circle, end point of a line, and so on. The value of this index depends on the specific type of graphic object; a value of -1 is considered to be an invalid key point.
If the mouse is over a graphic object when the mouse event occurs and the underlying application supports automatic key-point snapping, then this argument will contain the graphic.
Description
This event occurs when the mouse is clicked.
Syntax
Visual Basic
Public Function MouseClick( _
   ByVal sButton As Integer, _
   ByVal sShift As Integer, _
   ByVal dX As Double, _
   ByVal dY As Double, _
   ByVal dZ As Double, _
   ByVal pWindowDispatch As Object, _
   ByVal lKeyPointType As Long, _
   ByVal pGraphicDispatch As Object _
) As HResult
Parameters
sButton
Specifies on which button the click occurred. Valid values are vbLeftButton, vbRightButton, or vbMiddleButton.
sShift
Bitmask that determines the states of the Ctrl, Shift, and Alt keys when the mouse was clicked. For example, if both the Ctrl and Shift keys are pressed, the value is 6.
dX
Returns the x coordinate of the mouse in either the window or model coordinate system, depending on the value of the ScaleMode property.
dY
Returns the y coordinate of the mouse in either the window or model coordinate system, depending on the value of the ScaleMode property.
dZ
Returns the z coordinate of the mouse in the model coordinate system if the scale mode property is set to igMouseModel and the mouse event occurred in a graphic view; otherwise 0.
pWindowDispatch
Returns the window object in which the click event occurred.
lKeyPointType
If the mouse is over a graphic object when the mouse event occurs and the underlying application supports automatic key-point snapping, then this argument contains the index of the key point. Key points are significant points such as the center of a circle, end point of a line, and so on. The value of this index depends on the specific type of graphic object; a value of -1 is considered to be an invalid key point.
pGraphicDispatch
If the mouse is over a graphic object when the mouse event occurs and the underlying application supports automatic key-point snapping, then this argument will contain the graphic.
Remarks
The values of the constants are defined in the Visual Basic object library in the object browser. When a mouse click occurs in an application window, the MouseDown, MouseUp, and then MouseClick events are fired. In addition, the MouseClick event contains the same information that is contained in the MouseDown event.
See Also

ISEMouseEvents Object  | ISEMouseEvents Members