Solid Edge Framework Type Library
ScaleMode Property
Description
Sets and returns the scale mode.
Property type
Read-write property
Syntax
Visual Basic
Public Property ScaleMode As Long
Remarks
When set to 0, the scale mode is set to screen coordinates. When set to 1 (or anything other than 0), the scale mode is set to design space (model) coordinates.
See Also

ISEMouse Object  | ISEMouse Members