Solid Edge Framework Type Library
Active Property
Description
Sets and returns the name of the active style object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Active As String
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objLinearStyles As SolidEdgeFramework.LinearStyles
    Dim strActiveLinearStyle As String
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the LinearStyles object
    Set objLinearStyles = objDoc.LinearStyles
    'Get the Active LinearStyle name
    strActiveLinearStyle = objLinearStyles.Active
    'Change the Active LinearStyle
    objLinearStyles.Active = "Tangent"
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLinearStyles = Nothing
End Sub
See Also

LinearStyles Collection  | LinearStyles Members