Solid Edge Framework Type Library
Count Property
Description
Returns the number of objects in the referenced collection.
Property type
Read-only property
Syntax
Visual Basic
Public Property Count As Long
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objLinearStyles As SolidEdgeFramework.LinearStyles
    Dim lngcount As Long
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    'Get the LinearStyles object
    Set objLinearStyles = objDoc.LinearStyles
    'Get the count of LinearStyles already available
    lngcount = objLinearStyles.Count
    'Add few linearstyles
    objLinearStyles.Add Name:="LinearStyle1", Parent:="Tangent"
    Call objLinearStyles.Add(Name:="LinearStyle2", Parent:="Phantom")
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objLinearStyles = Nothing
End Sub
See Also

LinearStyles Collection  | LinearStyles Members