Solid Edge Framework Type Library : RibbonBarGroups Collection |
![]() | Returns the inserted item. The type of insert is defined by the mode parameter. For copy mode and move mode the inputs can be an object, a positive or negative integer index, or the string name of an item. For Create mode the first input must be a string. |
![]() | Returns an item in the collection. Valid inputs are a positive or negative integer index or the string name of the item. |
![]() | Removes the item. Valid inputs are an item object, a positive or negative integer index, or the string name of the item. |
![]() | Returns the active application object. |
![]() | Returns the number of objects in the referenced collection. |
![]() | Returns the parent object for the referenced object. |