Solid Edge Framework Type Library
Delivery Property
Description
Sets and returns the delivery method used when routing.
Property type
Read-write property
Syntax
Visual Basic
Public Property Delivery As RouteType
Remarks
The Delivery property is a read-write constant before routing starts and is read-only once routing is in progress.
See Also

RoutingSlip Object  | RoutingSlip Members