Solid Edge Framework Type Library
GetRouteInfo Method
Collapse All
Expand All
Solid Edge Framework Type Library
>
RoutingSlip Object
: GetRouteInfo Method
Description
Provides the user interface to gather the information for routing the associated document.
Syntax
Visual Basic
Public Function GetRouteInfo() As Boolean
Remarks
The user-specified routing information is set as properties in the RoutingSlip object. The method returns False when the dialog is cancelled.
See Also
RoutingSlip Object
|
RoutingSlip Members