Solid Edge Framework Type Library
Reset Method
Description
Clears RoutingSlip and Accelerator objects. For CommandBar objects, returns the built-in command bar to a default configuration.
Syntax
Visual Basic
Public Sub Reset() 
Remarks
If the RoutingSlip status is igRouteComplete, then the routing slip data remains after being reset, but with the current recipient as the originator; the status is reset to igNotYetRouted. All additional data from the slip is cleared.
See Also

RoutingSlip Object  | RoutingSlip Members