Solid Edge Framework Type Library
ReturnWhenDone Property
Description
Determines whether or not the associated document is returned to the originator after completing its route.
Property type
Read-write property
Syntax
Visual Basic
Public Property ReturnWhenDone As Boolean
Remarks
If True, the document is returned to the originator. Once routing is in progress, the ReturnWhenDone property becomes read-only.
See Also

RoutingSlip Object  | RoutingSlip Members