Solid Edge Framework Type Library
TrackStatus Property
Description
Specifies whether or not tracking is to be activated for the referenced RoutingSlip object.
Property type
Read-write property
Syntax
Visual Basic
Public Property TrackStatus As Boolean
Remarks
If this property is True, tacking is enabled. The TrackStatus property is read-write before routing begins; when routing starts, the property becomes read-only.
See Also

RoutingSlip Object  | RoutingSlip Members