Solid Edge Framework Type Library
Cut Method
Description
Moves the referenced object to the system clipboard.
Syntax
Visual Basic
Public Sub Cut() 
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objLine1 As SolidEdgeFrameworkSupport.Line2d
    Dim objLine2 As SolidEdgeFrameworkSupport.Line2d
    Dim objCircle1 As SolidEdgeFrameworkSupport.Circle2d
    Dim objSelectSet As SolidEdgeFramework.SelectSet
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' getting the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Create few 2d entities
    Set objLine1 = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.25, y2:=0.1)
    Set objLine2 = objSheet.Lines2d.AddByPointAngleLength(x:=0.1, y:=0.1, Angle:=45 / 180 * PI, Length:=0.25)
    Set objCircle1 = objSheet.Circles2d.AddByCenterRadius(x:=0.01, y:=0.01, Radius:=0.05)
    'Get hold of SelectSet object from Document object
    Set objSelectSet = objDoc.SelectSet
    'Add to SelectSet using Add method
    Call objSelectSet.Add(Dispatch:=objLine1)
    Call objSelectSet.Add(objCircle1)
    'Cut the SelectSet contents to ClipBoard
    objSelectSet.Cut
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objLine1 = Nothing
    Set objLine2 = Nothing
    Set objCircle1 = Nothing
    Set objSelectSet = Nothing
End Sub
See Also

SelectSet Collection  | SelectSet Members