| Solid Edge Framework Type Library > SolidEdgeTCE Object : CheckInDocumentsToTeamCenterServerEx Method |
This is a two dimensional array. Each row contains data per document. Each column will contain input information. For a document to be uploaded and checked in:
![]() |
Third and fourth columns are added in order to add the items to projects while doing checking of item in order to not break the existing APIs we make these parameters optional. |
Third and fourth columns are added in order to add the items to projects while doing check-in of item in order to not break the existing APIs we make these parameters optional.
| Visual Basic |
|---|
Public Sub CheckInDocumentsToTeamCenterServerEx( _ ByRef pvarFilesToBeCheckedInInfo As Variant, _ ByRef pvarArguments As Variant _ ) |
This is a two dimensional array. Each row contains data per document. Each column will contain input information. For a document to be uploaded and checked in:
![]() |
Third and fourth columns are added in order to add the items to projects while doing checking of item in order to not break the existing APIs we make these parameters optional. |
Third and fourth columns are added in order to add the items to projects while doing check-in of item in order to not break the existing APIs we make these parameters optional.
Option Explicit Sub Example() Dim objApplication As SolidEdgeFramework.Application Dim objTCE As SolidEdgeFramework.SolidEdgeTCE Dim SmartCodesInfo(1, 5) As Object Dim FilesToBeCheckedInInfo(1, 1) As Object Dim bUpload As Boolean Dim ObjArgs(0) As Object Set objApplication = GetObject(, "SolidEdge.Application") Set objTCE = objApplication.SolidEdgeTCE SmartCodesInfo(0, 0) = "Assign1" 'Input - Unique ID SmartCodesInfo(0, 1) = "Item" 'Input - Item Type SmartCodesInfo(0, 2) = Nothing 'Output ? Smart Code Number SmartCodesInfo(0, 3) = Nothing 'Output - Revision SmartCodesInfo(0, 4) = Nothing 'Output ? Container wise props in XML string SmartCodesInfo(0, 5) = Nothing 'Output ? Unget info in XML string SmartCodesInfo(1, 0) = "Assign2" 'Unique ID SmartCodesInfo(1, 1) = "Item" 'Item Type SmartCodesInfo(1, 2) = Nothing SmartCodesInfo(1, 3) = Nothing SmartCodesInfo(1, 4) = Nothing SmartCodesInfo(1, 5) = Nothing Call objTCE.GetSmartCodes(SmartCodesInfo) 'Example takes two documents to be checked in To Teamcenter. Caller should fill two 'dimensional array with two rows and two columns as filename and container wise props 'for smart code field set support. FilesToBeCheckedInInfo(0, 0) = "D:\300120.par" 'Cache Path FilesToBeCheckedInInfo(0, 1) = SmartCodesInfo(0, 4) FilesToBeCheckedInInfo(1, 0) = "D:\400120.par" 'Cache Path FilesToBeCheckedInInfo(1, 1) = SmartCodesInfo(1, 4) 'Set Boolean upload flag bUpload = False 'Fill array with first element with Upload flag. ObjArgs(0) = bUpload Call objTCE.CheckInDocumentsToTeamCenterServerEx(FilesToBeCheckedInInfo, ObjArgs) If Not objApplication Is Nothing Then Call objApplication.Quit End If Set objTCE = Nothing Set objApplication = Nothing End Sub