Solid Edge Framework Type Library > SolidEdgeTCE Object : OnUndoCheckOutDocuments Method |
The variant array which contains the file list to be UndoCheckOut.
Visual Basic |
---|
Public Sub OnUndoCheckOutDocuments( _ ByRef psaCacheFiles() As Variant _ ) |
The variant array which contains the file list to be UndoCheckOut.
Private Sub Command1_Click() On Error Resume Next Dim objApplication As SolidEdgeFramework.Application Dim objSolidEdgeTCE As SolidEdgeFramework.SolidEdgeTCE Set objApplication = GetObject(, "SolidEdge.Application") Set objSolidEdgeTCE = objApplication.SolidEdgeTCE Dim varInputList(1) As Variant varInputList(0) = "F:\016954.asm" varInputList(1) = "F:\016973.asm" Call objSolidEdgeTCE.OnUndoCheckOutDocuments(varInputList) Set objSolidEdgeTCE = Nothing Set objApplication = Nothing End Sub