| Solid Edge Framework Type Library > SolidEdgeTCE Object : SaveAsToTeamCenter Method |
Returns an array of following
1.Old ItemID and new ItemID
2.Old Revision and New Revision
3.Old Filename and New Filename
| Visual Basic |
|---|
Public Sub SaveAsToTeamCenter( _ ByVal bstrItemId As String, _ ByVal bstrItemRev As String, _ ByVal bstrDataSetFileName As String, _ ByVal bstrRevisionRule As String, _ ByVal bstrFolderName As String, _ ByRef pvarListOldAndNewItemIDRevsFileNames As Variant _ ) |
Returns an array of following
1.Old ItemID and new ItemID
2.Old Revision and New Revision
3.Old Filename and New Filename
Private Sub Command1_Click() On Error Resume Next Dim objApplication As SolidEdgeFramework.Application Dim objSolidEdgeTCE As SolidEdgeFramework.SolidEdgeTCE Dim objListFileNames As Object = Nothing Set objApplication = GetObject(, "SolidEdge.Application") Set objSolidEdgeTCE = objApplication.SolidEdgeTCE Dim FileItemID As String Dim FileItemRevID As String Dim FileDataSetName As String Dim FileRevisionRule As String Dim FolderName As String FileItemID = "020670" FileItemRevID = "A" FileDataSetName = "020670.par" FileRevisionRule = "Newstuff\SE\NewFolder" FolderName = "" Call objSolidEdgeTCE.SaveAsToTeamCenter(FileItemID, FileItemRevID, FileDataSetName, FileRevisionRule, FolderName, objListFileNames) Set objSolidEdgeTCE = Nothing Set objApplication = Nothing End Sub