Solid Edge Framework Type Library
Object Property
Description
Returns the dispatch interface associated with the site.
Property type
Read-only property
Syntax
Visual Basic
Public Property Object As Object
Remarks
The model automation of the source document depends on the type of the document. For example, the MS Word document automation and the MS Excel document automation are not the same.
See Also

Symbol2d Object  | Symbol2d Members