AspectRatio | Sets and returns aspect ratio of the text for the referenced TextCharStyle object. Value of aspect ratio must be greater than zero |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Color | Sets and returns the color in which the active object is drawn. |
Description | Returns a user-specified description of the referenced object. |
FontName | Sets and returns the font name for the referenced TextCharStyle object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
LangID | Sets and returns the language identification of the active text for the referenced TextCharStyle object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Style | Gets/Sets the Style of the text style (Bold, Italic, Bold Italic, Regular). |
TextSize | Sets and returns the size of the text for the referenced object. |
UnderlineStyle | Sets and returns the style of the underline for the referenced TextCharStyle object. |
Units | Sets and returns the units in which the line width is defined. |