Solid Edge Geometry Type Library
Cone Object Members
Overview 
Public Methods
Public Method GetAxisVectorReturns the unit vector that defines the axis of the referenced object.
Public Method GetBasePointReturns the center of the base of the referenced object.
Public Method GetConeDataReturns the surface geomtry data on the referenced cone object.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property ExpandingReturns True if the referenced object flares outward (increases in radius) progressing along the axis-vector from the basepoint.
Public Property HalfAngleReturns the acute angle subtended between the axis and a generator of the referenced cone.
Public Property ParentReturns the parent object for the referenced object.
Public Property RadiusReturns the radius of the referenced object.
Public Property TypeReturns a member of the GNTTypePropertyConstants set to indicate the type of the referenced object.
See Also

Cone Object