Solid Edge Geometry Type Library
Radius Property
Description
Returns the radius of the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Radius As Double
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBody As SolidEdgeGeometry.Body
    Dim objCone As SolidEdgeGeometry.Cone
    Dim sStatus As String
    Dim dblCnRadius As Double
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create a model (cone)
    sStatus = CreateModel(objDoc:=objDoc)
    If sStatus <> "" Then
        MsgBox sStatus
        Exit Sub
    End If
    ' Getting the Radius property of a Cone
    Set objBody = objDoc.Models(1).Body
    Set objCone = objBody.Shells(1).Faces(2).Geometry
    dblCnRadius = objCone.Radius

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objCone = Nothing
End Sub
See Also

Cone Object  | Cone Members