Solid Edge Geometry Type Library
GetDerivatives Method
Specifies the number of parameters to be evaluated.
Specifies the array of parameters at which to evaluate the curve.
Returns the first order partial derivative with respect to u.
Returns the first order partial derivative with respect to v.
Returns the second order partial derivatives with respect to u.
Returns the second order partial derivatives with respect to u and v.
Returns the second order partial derivatives with respect to v.
Returns the third order partial derivatives with respect to u.
Returns the third order partial derivatives with respect to v.
Description
Evaluates the derivatives of the referenced curve at the points given by an array of parameters on the curve.
Syntax
Visual Basic
Public Sub GetDerivatives( _
   ByVal NumParams As Long, _
   ByRef Params() As Double, _
   ByRef UPartials() As Double, _
   ByRef VPartials() As Double, _
   ByRef UUPartials() As Double, _
   ByRef UVPartials() As Double, _
   ByRef VVPartials() As Double, _
   ByRef UUUPartials() As Double, _
   ByRef VVVPartials() As Double _
) 
Parameters
NumParams
Specifies the number of parameters to be evaluated.
Params
Specifies the array of parameters at which to evaluate the curve.
UPartials
Returns the first order partial derivative with respect to u.
VPartials
Returns the first order partial derivative with respect to v.
UUPartials
Returns the second order partial derivatives with respect to u.
UVPartials
Returns the second order partial derivatives with respect to u and v.
VVPartials
Returns the second order partial derivatives with respect to v.
UUUPartials
Returns the third order partial derivatives with respect to u.
VVVPartials
Returns the third order partial derivatives with respect to v.
Remarks
The derivatives up to the third order can be output. You can choose to not obtain any of the derivatives by specifying a NULL in place of the corresponding output argument.
Example
Private Sub Form_Load()
    Dim objApp As solidedgeframework.Application
    Dim objDoc As SolidEdgepart.PartDocument
    Dim objBody As solidedgegeometry.Body
    Dim objFace As solidedgegeometry.Face
    Dim dblParams(1) As Double
    Dim dblUPartials() As Double
    Dim dblVPartials() As Double
    Dim dblUUPartials() As Double
    Dim dblUVPartials() As Double
    Dim dblVVPartials() As Double
    Dim dblUUUPartials() As Double
    Dim dblVVVPartials() As Double
    Const TESTFILE = "T:\vbtests\testcases\HalfCyl.par"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening the testfile
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting the body object of the model
    Set objBody = objDoc.Models(1).Body
    ' getting a particular face from the collection of faces on the body
    Set objFace = objBody.Faces(FaceType:=igQueryAll).Item(2)
    ' getting the derivatives at a point (u=0.5, v=0.5) on a Face
    dblParams(0) = PI / 2
    dblParams(1) = 0.05
    Call objFace.GetDerivatives(NumParams:=1, Params:=dblParams, UPartials:=dblUPartials, _
                                VPartials:=dblVPartials, UUPartials:=dblUUPartials, UVPartials:=dblUVPartials, _
                                VVPartials:=dblVVPartials, UUUPartials:=dblUUUPartials, VVVPartials:=dblVVVPartials)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBody = Nothing
    Set objFace = Nothing
End Sub
See Also

Face Object  | Face Members