Application | Returns the active application object. |
Area | Returns the area of the referenced object. |
Body | Returns the Body object for the referenced object. |
Continuity | Returns the continuity of the referenced object. |
Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. |
FacetCount | Returns the number of facets on the referenced object. |
Geometry | Returns a 3-D geometry object whose properties and methods can extend to the topology collection. |
GeometryForm | Specifies the geometry form of the referenced object. |
ID | Returns the Parasolid ID of the Face. |
IsParamReversed | Returns a Boolean value to specify whether or not the inherent direction of the referenced object is opposed to the flow dicated by the parameterization of the underlying geometry. |
Loops | Returns the Loops object collection for the referenced object. |
Parent | Returns the parent object for the referenced object. |
Shell | Returns the Shell object for the referenced object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
Tag | Returns the Tag of the Face. |
Type | Returns a member of the GNTTypePropertyConstants set to indicate the type of the referenced object. |
UpdatesCounter | Returns the number of times the referenced object has been modified. |
Vertices | Returns the Vertices object collection. |